Tool/software: TI-RTOS
Hi,
I had bought an AMIC110 ICE board. And I installed CCS7.2.0, Processor SDK RTOS for AM335x_v4.1.0, and PRU-ICSS-EtherCAT_Slave_01.00.05.00. I have rebuilt EtherCAT projects successfully, both demo version and full version.
Now I got the results as below:
1. If I run .out file of release version, there is not any LED on, not any print by UART, and TwinCAT could not recognize device.
2. If I run .out file of debug version, UART printed normal, TwinCAT can recognize device as Device 2 (EtherCAT), D2, D3, D4, and D17 on the board are on.However, there is only one LED under DO Outputs in TwinCAT Devices, and I could not control any LED by writeing online.
The UART print is as below:
Version - EtherCAT Slave 1.0.5.0
Board name : ICE110
Board Revision : 1.1
EtherCAT Device
SYS/BIOS EtherCAT Internal application 3.3.0
Revision/Type : x0190 Build : x04ec
Firmware Version : 1.4.236
Could some one give me some advices, please? Thanks.