Other Parts Discussed in Thread: TPS65218
I am trying to get the TFTP boot to work for the AM437x EVM board, but it doesn't seem to be working. I ran the setup script and get all the way through it, and at the end when it's supposed to run the minicom script and boot the board nothing happens. Minicom opens and just sits there and does nothing. I've tried both with the SD card plugged in and with it taken out, and both ways do not work. When the script gets to the point where you have to select which uImage you want to boot, I just select the default one. I'm not sure if this is right because there is no indication about which one I should be selecting or what the differences between all of them are. Any suggestions about what I could try to fix this issue are appreciated.