• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » ARM® Processors » Sitara™ ARM® » All Tags » AM3505/17
Share
Sitara™ ARM®
  • Forum
  • Announcements

Browse by Tags

Sitara™ ARM®

Welcome to the Sitara™ ARM® Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
AM3505/17
  • am3505
  • am3517
  • AM3517 boot
  • AM3517 datasheet
  • AM3517 EVM
  • AM3517 EVM Linux
  • am3517 som
  • am35x
  • AM35xx
  • am3715
  • boot
  • booting
  • cortex-a8
  • DDR2
  • Ethernet
  • GPIO
  • gpmc
  • kernel
  • linux
  • NAND
  • OMAP OMAP35xx AM35xx AM3517 EVM
  • sdk
  • Sitara
  • SPI
  • USB
Related Posts
  • Forum Post: Capability with MLC

    Hiroshi Kimizuka Hiroshi Kimizuka
    There is no description about MLC NAND in the AM35xx TRM. I would like to clarify that MLC is applicable to interface via GPMC in addition to SLC NAND ? H. KIMIZUKA
    on Dec 14, 2009
  • Forum Post: AM3505 Display Sub System ( DSS )

    MikeWilliams MikeWilliams
    I’ve read that the AM3505 DSS supports HD, but the datasheet is not clear about whether that is 720p or 1080p. There are a lot of TBD’s in that section. Is there any difference between the AM3505 and AM3517 in this area ? Are there any Preliminary App Notes / User Guide specifically...
    on Dec 29, 2009
  • Forum Post: AM3505 - USB3320 (Swap DP/DM) linux support

    Christoph Gollinger Christoph Gollinger
    Dear Community Members, We want to connect a USB3320 USB transceiver to the USB2/ULPI Interface and want to use linux. There is a Swap DP/DM feature that can be accessed by setting the respective bit in the vendor specific register 0x39(write). We want to set it to 1 in order to prevent crossing DP...
    on Jan 7, 2010
  • Forum Post: Using a Crystal with AM3517 (sys_xtalout and sys_xtalin pins)

    Alex Milgrom Alex Milgrom
    Hi All. I need information on the crystal that can be used on the sys_xtalout and sys_xtalin pins. The datasheet notes that a 26MHz Crystal or a 26MHz oscillator may be used here (defined by the sys_boot6 pin) but non of the reference designs I've seen uses a crystal (they all use an oscillator...
    on Jan 12, 2010
  • Forum Post: AM3505 power up sequence

    Jason2360 Jason2360
    Customer using AM3505, and we ran into a slight contradiction on something. The 3505 EVM and the 3505 datasheet list two different power up sequences. So I really just wanted to clarify, what is the correct power up sequence? Do you have that easily accessible, and can you please share that with me?
    on Jan 22, 2010
  • Forum Post: AM3517 - Booting up time from Flash after bypasing USB and UART3

    Pretesh Mascarenhas Pretesh Mascarenhas
    Hi, I am planning to place the AM35XX in our design. I needed some infomation in regards to Boot up time as thats one of our requirement. The set up: I am not using the UART or USB boot options I need the CPU to boot up from the external NAND flash (GPMC) in normal operation. However...
    on Feb 9, 2010
  • Forum Post: performance of video encoding on the AM3505

    Sebastian Kruber Sebastian Kruber
    Hi, for a new product I developed a video application on the OMAP 3530. It receives images from the ISP, encodes them in JPEG format and finally streams the video through USB. We are thinking about switching to the new AM3505 due to its 16bit camera interface and using ffmpeg library for video compression...
    on Feb 11, 2010
  • Forum Post: sys_clkreq pin ... a input or output ?

    Pretesh Mascarenhas Pretesh Mascarenhas
    Hi Say we are using an external CMOS digital clock through the sys_xtalin pin. In this case, the sys_clkreq is used as an output to request the external system clock. (1) Page 70 of datasheet – A CMOS digital clock through the sys_xtalin pin. In this case, the sys_clkreq is used as an output...
    on Feb 11, 2010
  • Forum Post: AM3517 DDR2 memory Manhattan lentghs

    miversen miversen
    Hi community, I have done Manhattan length calculations of a configuration with two DDR2 memories conected to AM3517. The AM3517 is placed at X,Y = 0,0 mm and the two DDR2 memories are placed at X,Yoffset = -44,+/-16 mm, which is the maximum allowable distance from AM3517 according to table 6-17 in the...
    on Feb 15, 2010
  • Forum Post: Graphics frame rate with EGL

    Tak Izaki Tak Izaki
    Hi, I have a trouble with frame rate of SGX530 graphics. I' now work on AM3517 EVM from LOGIC with Linux. I use SDK of Graphics. The frame rate of demo software seems 60Hz. I want to change the frame rate to 30 Hz. I believe eglSwapInterval() or PVRShellSet(prefSwapInterval, xx) can change...
    on Mar 17, 2010
  • Forum Post: real-time kernel patch

    Dominique Holzwarth Dominique Holzwarth
    hello is there a real-time kernel patch available for the kernel which is delivered with the PSP for the AM3517? currently i'm using the PSP 03.00.00.02 which has the kernel version 2.6.31-rc7. Update: The main reason why I have asked for a RT patch for the AM3517 PSP is because I've...
    on May 4, 2010
  • Forum Post: AM3517 Video Capture Driver

    Nhan Pham Nhan Pham
    HI, The current video capture driver doesn't support RGB input signal on the AM3517 application board. I wonder when will be one available for this input. Thanks Nhan Pham
    on May 10, 2010
  • Forum Post: DDR2 Termination

    fred50021 fred50021
    hi, is there an on-chip termination of the SDRC interface integrated in the am3505? in the am3505.pdf document on page 109 there are "T" symbols drawn on many lines. do they represent internal termination resistors and thus no additional termination is required (as always mentioned...
    on May 11, 2010
  • Forum Post: USB ports speed

    fred50021 fred50021
    hi, i am confused about the USB port speeds in the datasheets. It seams port0 ist the most comfortabel one to use. Can i use port0 as HS (480Mbps) host port for connecting USB Memory Sticks? thanks fred
    on May 12, 2010
  • Forum Post: About difference of function on the N21 and N22 pin.

    RY9983 RY9983
    Hello. We are one of the distributor of TI. Our customer is designing AM3517 system. Lately, new AM3517 datasheet was updated on TI web site. And, I found the functional difference of N21 and N22 pin in the new datasheet.(Table2-1, am3517.pdf) http://focus.ti.com/docs/prod/folders/print/am3517...
    on May 24, 2010
  • Forum Post: PCB Escape Routing for ZCN Package: mDDR/DDR2 connection

    Kentxu Kentxu
    In this link there's a very useful guide on routing the ZCN package: http://processors.wiki.ti.com/index.php/AM35x_VCA_PCB_layout Any possibility of continuing the design to show how to connect mDDR/DDR2 ? Also, it states that "The finished routing for this example is available...
    on Jun 22, 2010
  • Forum Post: Will there be any camera module supported for AM3517 EVM?

    Rich Chen Rich Chen
    Dear Sir, Is there any existed camera module (back end integrated, YUV output) supported for AM3517EVM? Alike Leopart and E-con we have for OMAP3530 EVM. If there is not, will any camera module be supported in the future. Best Regard, Rich
    on Jul 9, 2010
  • Forum Post: SYS_nRESWARM

    Andy Jump53114 Andy Jump53114
    I have been looking at both the Datasheet and Logic PD schematics for the AM35xx. There's a conflict between the two. The datasheet states that SYS_nRESWARM is open drain while page 2 of the SOM schematics from Logic PD states that it is open collector and no pull should be attached. I'm guessing...
    on Jul 21, 2010
  • Forum Post: 120fps VGA Video capture, storage and playback

    Calum Mackinnon Calum Mackinnon
    I have a customer looking for the following He wants 120fps camera and storage. Looks like the camera module outputs raw video 11 bits and is VGA @ 659x494 so a little over 0.3Megapixels per frame. So for him to get 120fps that's approx. 45Mpixel per second clock. He's looking for sub $10...
    on Aug 11, 2010
  • Forum Post: IBIS MODEL for AM35X

    Pretesh Mascarenhas Pretesh Mascarenhas
    Hi , I have downloaded the latest Ibis file for the AM3505/17 from TI's website. I need to carry out a pre placement simulation using Hyperlynx for the GPMC interface as this interface is connected to a multiple devices - FPGA, FLASH, Addr Latch. As such I need to determine the termination...
    on Aug 13, 2010
  • Forum Post: NOR flash for AM3505

    Anatoli Anatoli
    Can anyone please recommend 128 Mb (or just family) NOR flash part proven to boot AM3505?
    on Oct 2, 2010
  • Forum Post: ZCN Footprint - SMD or NSMD

    Andy Jump53114 Andy Jump53114
    I've ben looking at the ZCN footprint used on the AM35xx series and cannot determine whether this is intended to be used on a Soldermask Defined Pad PCB or Non-Soldermask Defined Pad PCB. The ball Diameter is given as 0.36mm to 0.46mm and the pad size on the downloadable footprint is 0.3mm. At the...
    on Oct 18, 2010
  • Forum Post: HECC bit timing of AM3157 is extended at ERM=1(Edge Resynchronization Mode)

    RY9983 RY9983
    Hello. I have encountered problem that HECC bit timing is extended at ERM=1. I confirmed it on AM3517EVM which just connect #2pin and #3pin of J36 on the application board. And I used AM35xx BSL and test program which can download in the Logic PD site. - 1013707A_AM35xx_BSL.zip\bsl\lib\evmam35xx_bsl...
    on Oct 30, 2010
  • Forum Post: About Windows CE BSP Lisence on AM3517

    RY9983 RY9983
    Hello. I am evaluating BSP_WINCE_ARM_A8-1.00.00.12. There are two types of lisence "TI Proprietary" and "Adeneo Proprietary" in the BSP. I would like to know about their detail. I have refered below. "BSP_WINCE_ARM_A8_1.00.00.12_Manifest.pdf : P9 Licenses" And, it describes...
    on Oct 30, 2010
  • Forum Post: MMC/SD support in AM3505

    Deepika Makhija Deepika Makhija
    As per sprugr0b.pdf, ROM code supports MMC/SD cards compliant with the Multimedia Card System Specification v4.2 from the MMCA Technical Committee and the SD I/O Card Specification v 2 .0 from the SD Association. Includes high-capacity (size >2GB) cards. What is the upper bound limit (if any...
    on Nov 2, 2010
1234
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use