• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » ARM® Processors » Sitara™ ARM® » All Tags » am335x
Share
Sitara™ ARM®
  • Forum
  • Announcements

Browse by Tags

Sitara™ ARM®

Welcome to the Sitara™ ARM® Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
am335x
  • 8bit nand
  • ADC
  • AM335
  • AM335 Linux
  • AM335 BeagleBone power
  • am335 boot NAND flash
  • AM335 Evaluation Board
  • am335 evm boot NAND flash
  • AM335 x
  • AM3352
  • AM3354
  • AM3357
  • AM3358
  • AM3358 EVM StarterKit JTAG
  • am3359
  • Am3359 AM335X DDR ram
  • AM3359 AM335X MCSPI SPI
  • am3359 beaglebone
  • AM3359 DDR
  • AM335x AM3359 DDR2
  • AM335x Boot USB
  • am335x ethercat profibus profinet sercos-iii powerlink
  • AM335x EVM
  • am335x_evm_config
  • android
Related Posts
  • Blog Post: Start your mission with the industry’s first $5 ARM® Cortex™-A8 microprocessor

    Russell Crane Russell Crane
    Imagine taking a handheld educational device based on an ARM9 processor and updating the product to include 3D interactive touch screen interfaces, higher resolution displays, better logic processing ability and wireless connectivity for multi-student interaction. This is all possible with TI’s...
    on Oct 31, 2011
  • Forum Post: Re: TMDXEVM3358 ( EVM )

    Lawrence Ronk Lawrence Ronk
    Hi Fabio, The AM335x EVM design files become available in mid-December. In the mean-time, check out the board design files for the AM335x based BeagleBone: http://beagleboard.org/hardware/design AM335x BeagleBone BeagleBone Rev A3 System Reference Manual Schematics (PDF) ...
    on Nov 16, 2011
  • Forum Post: AM335x complementary devices....

    uhtis uhtis
    Is there any pin compatible Dual core (ARM+DSP) device for AM335x just like the AM 1806 – L138 pair option?
    on Nov 22, 2011
  • Forum Post: Re: 512MB DDR2 memory with AM3359

    Miha Gostencnik Miha Gostencnik
    Hello, I've read EMIF section some more and saw that there is only one CS ("spruh73a.pdf", Section 7.3.1.2, Table7-98 States: Multiple DDR banks -> Only 1 CS/ODT pinned out) out of DDR memory controller. On BeagleBone board there is a 256MB(128Mx16) device with a 14bit Address...
    on Nov 24, 2011
  • Forum Post: Re: 512MB DDR2 memory with AM3359

    Miha Gostencnik Miha Gostencnik
    Hello, I somehow cant imagine using one CS with two devices, unless the other is negated. Because in Micron's datasheet states that "CS# enables (registered LOW) and disables (registered HIGH) the command decoder.". Therefore, how would memory controller know if both devices are accessed...
    on Nov 24, 2011
  • Forum Post: Re: AM335x WinCE ethernet based protocols / stack

    MPope MPope
    Is this something that I can sign up for under my registered software - like CE BSP for Omap35xx? Alpha EVM? Is it available with the AM3359 Industrial Communications Engine (ICE)? Will I only be able to get involved with this in Q1 - when in Q1? Thanks, Matt
    on Nov 29, 2011
  • Forum Post: AM335x support for Rapid Spanning Tree Protocol (RSTP)?

    Magnus Aman Magnus Aman
    Hi, I need your help to state what plans exist to support RSTP with AM335x? Please specifically state if this require special HW config (switch or dualmac mode) and what SW plans exist. (here: using Linux) Thanks. /Magnus
    on Dec 1, 2011
  • Forum Post: Re: AM335x and IEEE1588 drift

    Lawrence Ronk Lawrence Ronk
    Hi Magnus, The timestamp register in Sitara devices that support IEEE1588, like AM335x, is 32-bit wide. So, the limitation cited below is not applicable to Sitara devices. Regards, Lawrence
    on Dec 2, 2011
  • Forum Post: AM335x VGA output

    Marc Kellermann Marc Kellermann
    According to the datasheet the AM335x does not have a VGA output. Is it possible to convert the LCD controller "up to 24-bit data output" to a VGA output, so you can connect an external Display. If so can you recommend what external logic would be required. Thank you. -Marc Kellermann
    on Dec 4, 2011
  • Forum Post: Re: AM335x VGA output

    Lawrence Ronk Lawrence Ronk
    Hi Marc, Yes, use an external video encoder, like TI's THS8200. Regards, Lawrence
    on Dec 8, 2011
  • Forum Post: Re: AM3357,58 and 59

    Lawrence Ronk Lawrence Ronk
    Hi CherWei Sim: 1. Date available for the silicon (mass pro and engineering sample) For samples, today you can order the XAM3358ZCE and XAM3359ZCZ. Place sample orders from the product folder links: http://www.ti.com/product/am3357 http://www.ti.com/product/am3358 http://www.ti.com...
    on Dec 8, 2011
  • Forum Post: Re: AM335X's PRU support CMOS sensor?

    Lawrence Ronk Lawrence Ronk
    Hi Bobby, You might consider USB. Regards, Lawrence
    on Dec 8, 2011
  • Forum Post: Re: can Sitara (AM335x) mimic a USB device?

    Lawrence Ronk Lawrence Ronk
    Hi Julius, 1. Can Sitara (AM335x) mimic a USB device? Yes, the AM335x has integrated USB OTG ports that can function as USB Device or USB Host. Note that both the USB controllers and the USB Phy’s are integrated. Please refer to the device datasheet for details. 2. Where can I...
    on Dec 9, 2011
  • Forum Post: Re: Linux Rt support?

    Lawrence Ronk Lawrence Ronk
    Hi Dave, You can find some information and pointers on RT Linux at the following wiki: http://processors.wiki.ti.com/index.php/Realtime Also, for details about RT-preemption patch development and status it is recommended to visit the RT Wiki and/or follow the developer list (rtlist-at-vger). The...
    on Dec 9, 2011
  • Forum Post: AM335x - Lowest possible power without using standby/sleep modes

    D. Johnson D. Johnson
    We would like to understand the operation under lowest possible power conditions. Some of the things we might like to do are: - Run the processor as SLOW as possible - Not use any dynamic memory (mDDR, DDR2, etc) - Run code from external memory such as Flash and possibly SRAM. Now on to...
    on Dec 9, 2011
  • Forum Post: what do AM35X family have which is not in possession of AM335X family?

    mikhail lodigin mikhail lodigin
    I'm in trouble to separate AM35X family from AM335X family. In my opinion AM335X is like continuation of AM35X. but since it is different family WHY it is different? I believe I miss something but what? thank you.
    on Dec 12, 2011
  • Forum Post: Re: what do AM35X family have which is not in possession of AM335X family?

    Lawrence Ronk Lawrence Ronk
    Mikhail, Check-out the device migration guide for a feature comparison between AM35x and AM335x. Links to AM35x to AM335x Migration Guide: AM35x to AM335x Hardware Migration Guide http://processors.wiki.ti.com/index.php/AM35x_To_AM335x_Hardware_Migration_Guide Note that links to Migration...
    on Dec 12, 2011
  • Forum Post: AM335x - long time support?

    Miha Gostencnik Miha Gostencnik
    Hello, I have a question regarding availability and support for AM335x processors; mainly how long do you plan to have them in production (for example, next 3, 5, 6, or more years)? Thank you very much for you help and have a nice day. Best regards, Miha
    on Dec 13, 2011
  • Forum Post: Re: Solution for NAND flash controller

    Lawrence Ronk Lawrence Ronk
    Ayus, The AM335x has an integrated NAND Flash Controller. Please refer to the AM335x Data Manual and AM335x Technical Reference Manual for a description of the NAND Flash Controller. You can download these documents from the AM335x Product Folders: http://www.ti.com/product/am3358 Also, a Linux...
    on Dec 14, 2011
  • Forum Post: BeagleBone Android performance with micro SD and micro SDHC cards

    Binh Nguyen Binh Nguyen
    I have tested BeagleBone board (AM3359) with different micro SD cards and here are what I found: 1. With a Sandisk micro SD 2GB card, Android boot time is excellent (first boot or subsequent boots). With this micro SD, Android apps in rowboPERF were carried out quickly. 2. If Android image installed...
    on Dec 14, 2011
  • Forum Post: Re: BeagleBone Android performance with micro SD and micro SDHC cards

    Miha Gostencnik Miha Gostencnik
    Hello Binh, you could try a new release if it helps: http://processors.wiki.ti.com/index.php/AM335x-PSP_04.06.00.03_Release_Notes . As it is written on the page, it fixes some bugs with certain SD cards ("Beaglebone : Board loses power with certain SD cards"). Have a nice day, Miha
    on Dec 15, 2011
  • Forum Post: Re: AM335x - long time support?

    Miha Gostencnik Miha Gostencnik
    Hello, I am mainly asking this because I'm designing a new product and availability would be a good to know :), so I can "sell" this information to potential buyers/firms. Best regards, Miha
    on Dec 21, 2011
  • Forum Post: uImage-am335x-evm.bin not loading (beaglebone)

    Bill Crupi Bill Crupi
    I am getting the following messages: U-Boot# reset resetting ... U-Boot SPL 2011.09 (Nov 04 2011 - 21:43:12) Texas Instruments Revision detection unimplemented No AC power, disabling frequency switch OMAP SD/MMC: 0 reading u-boot.img reading u-boot.img U-Boot 2011.09 (Nov 04 2011 - 21:39:19) I2C:...
    on Dec 26, 2011
  • Forum Post: Re: AM335x and IEEE1588 drift

    James McCartney92666 James McCartney92666
    In addition to drift which I will assume is directly related to the quality of the oscillator used in the system, do you have any measurements on stability of the IEEE 1588 PTP subsystem. Specifically you know of anyone who has made Allen Deviation measurements on the steered frequency? It would be interesting...
    on Jan 2, 2012
  • Forum Post: Re: AM335x and DDR3

    Viral Sachde Viral Sachde
    Hi Lawrence and other people at TI, Can some one suggest me where is this 'Data Manual' ? Viral
    on Jan 2, 2012
12345»
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use