• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » ARM® Processors » Sitara™ ARM® » All Tags » am3517
Share
Sitara™ ARM®
  • Forum
  • Announcements

Browse by Tags

Sitara™ ARM®

Welcome to the Sitara™ ARM® Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
am3517
  • am3505
  • AM3505/17
  • AM3517 boot
  • AM3517 datasheet
  • AM3517 EVM
  • AM3517 EVM Linux
  • am3517 som
  • am35x
  • AM35xx
  • am3715
  • android
  • boot
  • Boot sequence.
  • booting
  • camera
  • clock
  • cortex-a8
  • DDR2
  • DM3730
  • flash
  • GPIO
  • gpmc
  • I2C
  • JTAG
  • kernel
Related Posts
  • Forum Post: How are the Cortex-A8 based Sitara AM3505 and AM3517 optimized for the industrial market?

    Phillip Parker Phillip Parker
    First ARM Cortex-A8 processor based solution optimized for industrial market, delivering greater ARM performance than previous alternatives in the market. Peripherals including CAN controller and Ethernet MAC as well as industrial temperature-grade options and package alternatives to enable developers...
    on Oct 20, 2009
  • Forum Post: What is the roadmap for OMAP3503/3515 devices?

    Phillip Parker Phillip Parker
    OMAP3503/15 - Sitara AM3505, AM3517 or AM Next generation devices depending on your needs. There will also be future ARM Cortex-A8 based products in the Sitara family that will offer higher performance and lower cost alternatives.
    on Oct 20, 2009
  • Forum Post: What is the roadmap for OMAP3525/OMAP3530 devices?

    Phillip Parker Phillip Parker
    OMAP3530/3525 -Future DM based deviceswill provide similar functionality as the OMAP3530 and 3525. Beyond these, there are several high-performance, multimedia-focused devices in the DaVinci platform that are in development that will offer even greater video and media performance. These devices will...
    on Oct 20, 2009
  • Forum Post: multichannel audio application on 3517/05

    Yan8622 Yan8622
    On 3517/05 , are there enough I2S (or compatible) to handle 8-in/8-out audio channels, for example in a portable mixing console?
    on Nov 19, 2009
  • Forum Post: AM3505 - USB3320 (Swap DP/DM) linux support

    Christoph Gollinger Christoph Gollinger
    Dear Community Members, We want to connect a USB3320 USB transceiver to the USB2/ULPI Interface and want to use linux. There is a Swap DP/DM feature that can be accessed by setting the respective bit in the vendor specific register 0x39(write). We want to set it to 1 in order to prevent crossing DP...
    on Jan 7, 2010
  • Forum Post: Using a Crystal with AM3517 (sys_xtalout and sys_xtalin pins)

    Alex Milgrom Alex Milgrom
    Hi All. I need information on the crystal that can be used on the sys_xtalout and sys_xtalin pins. The datasheet notes that a 26MHz Crystal or a 26MHz oscillator may be used here (defined by the sys_boot6 pin) but non of the reference designs I've seen uses a crystal (they all use an oscillator...
    on Jan 12, 2010
  • Forum Post: AM3517: Recommended operating voltage specs

    Mark Utter Mark Utter
    The current AM3517 datasheet only specifies nominal recommended operating voltages for the device. Customer is in design and needs to know min and max for VDDCORE. The nominal VDDCORE is specified as 1.2V. They using the TPS65023. Due to a workaround, the VDDCORE comes up at 1.225V instead of 1.20V...
    on Jan 19, 2010
  • Forum Post: AM3517 - Booting up time from Flash after bypasing USB and UART3

    Pretesh Mascarenhas Pretesh Mascarenhas
    Hi, I am planning to place the AM35XX in our design. I needed some infomation in regards to Boot up time as thats one of our requirement. The set up: I am not using the UART or USB boot options I need the CPU to boot up from the external NAND flash (GPMC) in normal operation. However...
    on Feb 9, 2010
  • Forum Post: sys_clkreq pin ... a input or output ?

    Pretesh Mascarenhas Pretesh Mascarenhas
    Hi Say we are using an external CMOS digital clock through the sys_xtalin pin. In this case, the sys_clkreq is used as an output to request the external system clock. (1) Page 70 of datasheet – A CMOS digital clock through the sys_xtalin pin. In this case, the sys_clkreq is used as an output...
    on Feb 11, 2010
  • Forum Post: AM3517 DDR2 memory Manhattan lentghs

    miversen miversen
    Hi community, I have done Manhattan length calculations of a configuration with two DDR2 memories conected to AM3517. The AM3517 is placed at X,Y = 0,0 mm and the two DDR2 memories are placed at X,Yoffset = -44,+/-16 mm, which is the maximum allowable distance from AM3517 according to table 6-17 in the...
    on Feb 15, 2010
  • Forum Post: Graphics frame rate with EGL

    Tak Izaki Tak Izaki
    Hi, I have a trouble with frame rate of SGX530 graphics. I' now work on AM3517 EVM from LOGIC with Linux. I use SDK of Graphics. The frame rate of demo software seems 60Hz. I want to change the frame rate to 30 Hz. I believe eglSwapInterval() or PVRShellSet(prefSwapInterval, xx) can change...
    on Mar 17, 2010
  • Forum Post: AM3517 EVM + Application board uboot issue

    Diego Chaverri Diego Chaverri
    Hi, I'm working with an AM3517 EVM Development Kit. I'm having trouble when connecting the Application board to the EVM, I get the following message: Texas Instruments X-Loader 1.45 (Mar 19 2010 - 19:44:22) Starting X-loader on MMC Reading boot sector 214940 Bytes Read from MMC Starting OS...
    on Apr 14, 2010
  • Forum Post: real-time kernel patch

    Dominique Holzwarth Dominique Holzwarth
    hello is there a real-time kernel patch available for the kernel which is delivered with the PSP for the AM3517? currently i'm using the PSP 03.00.00.02 which has the kernel version 2.6.31-rc7. Update: The main reason why I have asked for a RT patch for the AM3517 PSP is because I've...
    on May 4, 2010
  • Forum Post: AM3517 Video Capture Driver

    Nhan Pham Nhan Pham
    HI, The current video capture driver doesn't support RGB input signal on the AM3517 application board. I wonder when will be one available for this input. Thanks Nhan Pham
    on May 10, 2010
  • Forum Post: DDR2 Termination

    fred50021 fred50021
    hi, is there an on-chip termination of the SDRC interface integrated in the am3505? in the am3505.pdf document on page 109 there are "T" symbols drawn on many lines. do they represent internal termination resistors and thus no additional termination is required (as always mentioned...
    on May 11, 2010
  • Forum Post: USB ports speed

    fred50021 fred50021
    hi, i am confused about the USB port speeds in the datasheets. It seams port0 ist the most comfortabel one to use. Can i use port0 as HS (480Mbps) host port for connecting USB Memory Sticks? thanks fred
    on May 12, 2010
  • Forum Post: About difference of function on the N21 and N22 pin.

    RY9983 RY9983
    Hello. We are one of the distributor of TI. Our customer is designing AM3517 system. Lately, new AM3517 datasheet was updated on TI web site. And, I found the functional difference of N21 and N22 pin in the new datasheet.(Table2-1, am3517.pdf) http://focus.ti.com/docs/prod/folders/print/am3517...
    on May 24, 2010
  • Forum Post: AM3517 DDR Connection clarification

    John Bukowski John Bukowski
    The portion of the AM3517 datasheet that explains how to route the DDR portion of the PCB is on pages 135-147. My question is: If we had to choose between “T-routing” the control lines OR the address lines, which set should we “T”?
    on Jul 20, 2010
  • Forum Post: AM3517 - 26MHz Voltage Level

    Dave Pulvermacher Dave Pulvermacher
    If my 26MHz signal is oscillating between 0 and 1v, is that enough to drive the uP? VDDSHV = 3.3V. My oscillator is being powered by 1.8v so I expect to be higher but, alas, it isn't. thanks
    on Aug 17, 2010
  • Forum Post: DDR_PADREF

    Dave Pulvermacher Dave Pulvermacher
    I just realized that I do not have the DDR_PADREF (B12) line pulled down on my board (it's floating). How bad is this? Is there any way I can still use the DDR?
    on Aug 20, 2010
  • Forum Post: 32.768kHz for AM3517

    Dave Pulvermacher Dave Pulvermacher
    What voltage level should an external 32.768kHz oscillator be running at? My confusion stems from the EVM being at 3.3V but the wiki page states 1.8V (see below). If the 32KHz oscillator you choose exceeds the rise/fall time limit, a push-pull output buffer should be used to create a faster...
    on Aug 24, 2010
  • Forum Post: Using POWER_ON to reset AM3517 board

    Dave Pulvermacher Dave Pulvermacher
    I put a switch in to pull POWER_ON (from the TPS650732) low (it is otherwise pulled up to Vsys). I would still like to tie POWER_ON to the AM3517, though, in order to give the 3517 the ability to reset the board. I see on a ref schematic that POWER_ON is going into a GPIO on the 3517. My only concern...
    on Aug 26, 2010
  • Forum Post: Unable to Read and write in External NAND[AM3517].

    hrishikesh choudhary hrishikesh choudhary
    Dear All, We have a custom board which has AM3517 controller interfaced to External NAND through FPGA. The Control signal and Data signal are routed through FPGA to NAND. Currently I am trying to Read ID from the NAND . But whatever value i write to the NAND in the form of Command is reflected back...
    on Apr 27, 2012
  • Forum Post: State of SYS_NRESWARM after the reset

    Daisuke Maeda Daisuke Maeda
    http://processors.wiki.ti.com/index.php/AM35x_Schematic_Checklist#RESETS I saw the following description in the above Wiki. 1. SYS_NRESWARM is pulled-low when SYS_NRESPWRON is LOW. 2. Once SYS_NRESPWRON goes HIGH, for PRM_RSTTIME, SYS_NRESWARM will be driven LOW (No pull down). 3. After that SYS_NRESWARM...
    on May 10, 2012
  • Forum Post: VDDS_DSI and AM3505 - Is there a need for a VDDS_DSI regulator?

    Raphaël Assénat Raphaël Assénat
    Hello, We ran into an issue where the Linux omapdss driver would refuse to run because it couldn't find a VDDS_DSI regulator. Our design does not have such a regulator because it seems there is no such thing as an VDDS_DSI input pin. I made a patch to prevent searching and using a regulator on...
    on Jul 19, 2012
12345»
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use