• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » ARM® Processors » Sitara™ ARM® » All Tags » linux
Share
Sitara™ ARM®
  • Forum
  • Announcements

Browse by Tags

Sitara™ ARM®

Welcome to the Sitara™ ARM® Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
linux
  • AM335
  • AM335 Linux
  • AM335 x
  • AM3358
  • am3359
  • am3359 beaglebone
  • am335x
  • AM335x EVM
  • am3505
  • AM3505/17
  • am3517
  • AM3517 boot
  • AM3517 datasheet
  • AM3517 EVM
  • AM3517 EVM Linux
  • am35x
  • AM35xx
  • am3715
  • am37x
  • AM37xx
  • android
  • beaglebone
  • boot
  • booting
  • cortex-a8
Related Posts
  • Blog Post: TI adds two new MPUs to the Sitara™ family

    Russell Crane Russell Crane
    Monday, June 7, we announced two new Sitara AM37x MPU devices, the AM3715 and AM3703. These new 1GHz Cortex-A8 processors offer design flexibility and compatibility for a variety of high-performance, low-power applications. What is so different about the AM37x compared to our other MPUs? The...
    on Jun 9, 2010
  • Forum Post: AM35x Software Q&A

    Alan Neidig Alan Neidig
    Had a few software questions for AM35x devices ... Linux with drivers for ALL peripherals ? If not all, which one(s) are missing? Complete BSP for Linux ? Support for creating native libraries to support Java ? Cross compilation and debugging support ? JAVA JVM support (full sun java implementation...
    on Jun 22, 2010
  • Forum Post: TMDXEVM3730: SPI access and sample code?

    Jeffrey Graham Jeffrey Graham
    Hello, About to order the dev kit. Does it provide access to SPI, and is there example code showing usage (Linux)? Thanks, Jeff
    on Aug 23, 2010
  • Forum Post: TMDEXVM3730: ${DVSDK}/setup.sh (updated)

    Jeffrey Graham Jeffrey Graham
    Hello, Just received my TMDEXVM3730 kit, and am having trouble with the setup.sh script. I am trying to follow the instructions in the TMS320DM3730 Software Developers Guide". I am running Windows XP Pro on an HP laptop, and using VMPlayer to provide my Ubuntu 10.04 LTS environment....
    on Sep 27, 2010
  • Forum Post: AM3517 HDMI driver for Linux

    Ken Sanchez Ken Sanchez
    We have a need for 720p video thru an HDMI port. Is there a linux driver for an HDMI controller? If so, is it in a board support package? Thanks, Ken
    on Oct 15, 2010
  • Blog Post: CraneBoard for the Holidays!

    Russell Crane Russell Crane
    Just in time for the holidays, Mistral announced a new low-cost ARM® based development board for developers utilizing Texas Instruments’ AM35x Sitara™ ARM Cortex-A8™ microprocessor (MPU). Dubbed the CraneBoard, the new ARM-based open source development is a cost-effective alternative...
    on Dec 17, 2010
  • Forum Post: Very annoyed with the AM3517 ROM Loader

    Michael Erickson Michael Erickson
    Hello all, I've been having some highly mixed results booting from an SD Card on the AM3517. I've read everything that I can on the wikis and in the manual. Using fdisk, 99% of the time I can successfully create a bootable card, populate it with MLO, u-boot.bin, etc. etc. and all is well...
    on Jan 21, 2011
  • Forum Post: AM35xx in network applications (design considerations)

    Leandro Santos Leandro Santos
    Hi developers, I have an application where the processor must operate as a router. So I need: Linux Kernel does packet forwarding (this requirement may be heavy to ARM architecture) Port Quagga to use OSPF (to update routing table) I'm interested to know: Does it exist routers...
    on Jan 25, 2011
  • Forum Post: Customizing Power States

    Justin Forrester Justin Forrester
    I am in the process of configuring the AM3517 SOM-M2 to run in a very low power sleep mode. So far the lowest I have been able to go is 20mA. My goal is to achieve a 1mA or lower sleep current draw. The supplier, LogicPD, has confirmed that this is possible, but it may require building the power state...
    on Jan 26, 2011
  • Forum Post: Changing from 500MHz to 600MHz in Linux kernel

    Mugen Mugen
    Hello. How to change cpu frequency in linux kernel from 500MHz to 600MHz without using cmdline mpurate=600M? What file in kernel source I have to change ? With cmdline mpurate=600M kernel tells that it switch into new frequency 600Mhz but BogoMips remains 499,92 and there is no effect of using...
    on Jan 29, 2011
  • Forum Post: new linux kernel with functioning dsp and c6run examples for tmdxevm3730 (by Mistral)

    Jeffrey Graham Jeffrey Graham
    Hello, I am trying to get the DSP working with both my TI AM/Dm3730 Evaluation Module (part # TMDXEVM3730 purchased 6 months ago) and an Overo Fire board, using c6Run and its examples. Focusing just on the TI board, I have tried with the 2.6.32-psp03.00.01.06 kernel (in the dvdsdk_dm3730-evm_4_01_00_09...
    on Mar 15, 2011
  • Forum Post: Why does the AM3517 UART4 can only send not receive ?

    mike wang70980 mike wang70980
    Hi, I have modified the linux kernel 03.00.00.04 by enable_uart4_am3517.txt. IRQ = 84, memory base = 0x4809e000, IO port multiplexing mode is set, but is not receiving data. UART4_RX , GPIO_133 output is correct, the right connections. It is said to be enabled fck, bit 23 of PRCM...
    on Apr 7, 2011
  • Forum Post: Help with GPIO via SYSFS on AM3517 EVM

    Chris Hartley Chris Hartley
    I'm trying to do some simple GPIO in linux. If I have read things correctly (including schematics) I should be able to do the following to change the USERLED3 on the EVM: ------------------- root@am3517-evm:~# cd /sys/class/gpio/ root@am3517-evm:/sys/class/gpio# echo 11 > export root@am3517...
    on Apr 21, 2011
  • Forum Post: AM3517 booting or flashing kernel via tftp issue

    Aaron Ridinger Aaron Ridinger
    Hello, I'm trying to load the default kernel from the PSP on an AM3517 on a Logic PD experimenter board. I'm running Ubuntu 9.04 on Virtual Box on Windows 7. I think the issue is with the TFTP, as it won't get past that step. I've tried both flashing the kernel via tftp, and booting...
    on Apr 27, 2011
  • Forum Post: TFTP Server Settings in Ubuntu VMware 11.04 Latest version(LINUX)

    francis kumar francis kumar
    Hi all, I am facing problem with TFTP booting. It is not loading the kernal(uImage) in my target. I have installed all the TFTP & XINETD packages in my Linux host machine. My Host Machine Details : Ubuntu VMware 11.04 Latest version(LINUX). Target Details : AM1808(TI Sitara) root...
    on May 21, 2011
  • Forum Post: Setting up a NFS client on AM35xx EVM outside uBoot

    Marc Pelletier Marc Pelletier
    Hi, I have successfuly setup the eXperimenter Dev kit to boot from the SD Card, with the file system on it (two partitions...). This took a bit of time but is working fine now. I want to use NFS to mount a folder from the Ubuntu development computer, to debug and make easy file transfers to/from...
    on May 25, 2011
  • Forum Post: Prevent Kernel from De-initing LCD at Boot

    David Paden David Paden
    I am using the AM3517 with Linux. I have enabled the LCD at boot with U-Boot to show a splash screen, and the LCD is working fine once Linux is up and running. However, in the time between U-Boot handing off operation to the Kernel and the Kernel re-initializing the LCD (DSS, DISPC, DPI), the LCD...
    on Jun 1, 2011
  • Forum Post: CCSv5 Connection Refused Remote System Explorer or SSH To LogicPD AM3517 Experimenter

    meg meg
    I am using the LogicPD AM3517 Experimenter board - trying to connect to it's Ethernet port from CCSv5 (Version: 5.0.1.201012231000) on Ubuntu Linux 10.04. I installed Remote System Explorer in CCSv5 but no dialog came up regarding security file like the example. Can connect to AM3517 Experimenter...
    on Jun 9, 2011
  • Forum Post: AM3517 Experimenter SDK SD Card Boot Hangs On Calibrating Touchscreen

    meg meg
    I have a LogicPD AM3517 Experimenter board. This comes with a minimal Linux installation. It was suggested that I create an SD Card boot of the latest Linux SDK for Sitara which I did. The version is at http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/sdk/AM3517/latest/index_FDS...
    on Jun 11, 2011
  • Forum Post: AM3517 CAN Interface (Changing bitrates)

    Justin Forrester Justin Forrester
    Normal 0 false false false EN-US X-NONE X-NONE MicrosoftInternetExplorer4 ...
    on Jul 6, 2011
  • Forum Post: The ZOOM AM3517 can't launch Linux system

    token token
    hi , I have setup ti-sdk-am3517-evm-05.02.00.00-Linux-x86-Install.and compile the AM3517 linux system (linux-2.6.37-psp04.02.00.07) like this: 1. make ARCH=arm CROSS_COMPILE=arm-arago-linux-gnueabi- distclean 2. make ARCH=arm CROSS_COMPILE=arm-arago-linux-gnueabi- am3517_evm_defconfig 3....
    on Jul 21, 2011
  • Forum Post: AM3715 SPI Driver for Linux?

    Yves McDonald Yves McDonald
    Hello, I'm currently working on an embedded software application for an embedded medical device. The device uses the Sitara AM3715 system on chip. That chip uses its McSPI interface #1,0 to communicate with a FPGA, which will do much of the I/O processing. The embedded application runs under Linux...
    on Jul 26, 2011
  • Forum Post: AM3517 uptime issue (goes forward 2^17 seconds)

    Paolo Pellegatti Paolo Pellegatti
    Hi All, We are using TI PSP 03.00.01.06 (Kernel 2.6.32) on Variscite board SOM-AM35. The uptime (and also the system clock with date command) goes forward of exactly of 2^17 seconds without any user interaction/application. We normally notice this time warp after 2 days since when the terminal is...
    on Jul 29, 2011
  • Forum Post: AM3517 McSPI1 driver does not seem to work in Linux

    Yves McDonald Yves McDonald
    The problem I have is that sPI signals don't seem to get on the i/o connector pins dedicated to McSPI bus #1. After investigating the problem, I found which Linux kernel source file was doing BGA ball assignment and mux'ing. The file in question is mux34xx.c . [ref.1] Since the kernel was...
    on Aug 3, 2011
  • Forum Post: AM3517 EEPROM - I2C Problem

    Onder Sanane Onder Sanane
    Hi, altough I can see i2c-1 , i2c-2 and i2c-3 under the /dev directory, I am not able to read the eeprom via i2c-1. In the documentations it is stated that the eeprom is attached to i2c-1. The device address of eeprom starts with 1010 and default eeprom address is stated as 000 for i2c. So, the...
    on Aug 23, 2011
12345
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use