This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TAS5720A-Q1: Amplification for signal >20kHz

Expert 6675 points

Replies: 6

Views: 264

Part Number: TAS5720A-Q1

Hi Team,

I am looking for an audio amplifier that can handle a signal bandwidth above the audio band, up to 75kHz. Is this a limitation that is set by the audio amplifier itself, or the output LC filter?

I took a look at the TAS5720A-Q1, and it look like the perfect device b/c it is class-D, mono output, and can produce >20W, but I am not sure if it can handle a signal up at 75kHz.. any insight you can provide would be greatly appreciated. 

Thank you for your support!

-Jared

  • Hi Jared,
    Actually our closed-loop class-d products are being widely used in the ultra-sound apllication. It can support upto 75kHz loop bandwidth, but you need to redesign the LC output filter. Do you have TAS5720M EVM board? You can do filter tuning on that board.
    Best regards,
    Shawn Zheng
  • In reply to Shawn Zheng:

    Hi Shawn,

    Thank you for the speedy reply! Can I use this calculator to select my LC filter values?

    Good to know about the EVM, I will check it out!

    Thanks!

    Jared

  • In reply to Jared Becker:

    Hi Jared,
    You can use that calculator, but it's only a simplified model(pure resistance load). The real load is usually more complex(including inductance, capacitance). Anyway the result got from this should be a good tuning start point.
    Best regards,
    Shawn Zheng
  • In reply to Shawn Zheng:

    Hi Shawn,

    Thank you for the note. If I am looking for the same thing, but analog input, do you know if the TAS5421 would work at the higher bandwidth?

    I appreciate your insight. thanks!

    Jared

  • In reply to Jared Becker:

    Hi Jared,

    I'm sorry I'm not familiar with TAS5421Q1, could you please creat a new post with TAS5421Q1 in title in the forum? Then our application expert in this device will give professional answers. Thank you!

    Best regards,

    Shawn Zheng

  • In reply to Shawn Zheng:

    No worries, thank you Shawn!

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.