This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TAS2521: Can it be used without MCLK?

Intellectual 600 points

Replies: 1

Views: 73

Part Number: TAS2521

Hello TI team

The TAS2521 has a PLL function inside. If DAC_CLK is used with BCLK, do not need to input an external MCLK?

or do I have to input MCLK?

  • Hi Downey,

    MCLK is optional for TAS2521. As you say, you can select BCLK as input to the PLL to set the internal sampling frequency.
    This is as shown in Application Reference Guide section 2.6 and figure 2-8: www.ti.com/.../slau456.pdf

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.