This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TPA2000D1-Q1: Issue with audio amplifier

Prodigy 20 points

Replies: 2

Views: 172

Part Number: TPA2000D1-Q1

Hi there,

I am using TPA2000D1TPWRG4Q1 along with 6PAIC3109TRHBRQ1, I could not get sound at the audio amplifier output, I have connected speaker at CODEC output it, Sound is coming. but, at the amplifier output it is not coming. could any one solve my issue, attached the schematic for reference.

Thank you.

Regards,

Uttej Ravuri.

  • Hi Uttej,

    Do you have captures of the signals around the device? I mean input signals at INP/INN, output signals at OUTP/OUTN before and after the output filter. Perhaps also the Shutdown signal would be good to see as well.

    I think the first thing to look at is the output, this is a Class-D amplifier so there should be a PWM at the output at least if the device is operating.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators
  • In reply to Ivan Salazar:

    Hi Uttej,

    Do you have further comments about the above?
    If your application has been solved please let us know so we can close this thread.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.