This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

PCM2912A: How Can We Configure the PCM2912A's to Max Output Volume in Default?

Genius 12400 points

Replies: 5

Views: 178

Part Number: PCM2912A

Hi Sirs,

With inbox UAC driver, can we configure the PCM2912A to maximum output volume in default?

Thank you and Best regards,

Wayne Chen
01/09/2019

  • Hi, Wayne,

    From the PCM2912A point of view, there is no way to configure a default Volume value, it is determined by the host device. I don't know if the UAC driver can be configured to have a given default volume setting, that is something which should be verified directly on the host device .

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer

  • In reply to Diego Melendez:

    Thank you for your confirmation, Diego...Wayne Chen
  • In reply to Wayne Chen (ODM FAE):

    Hello Diego,

    Addition, does the PCM2912A device's default settings factory programmable? Or can we offer software tools for customers to patch it?

    Thank you and Best regards,

    Wayne Chen
    01/11/2019  

  • In reply to Wayne Chen (ODM FAE):

    Hi, Wayne,

    Unfortunately there is no way to re-program the PCM2912A's default factory settings.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer

  • In reply to Diego Melendez:

    Thanks a lot, Diego...Wayne Chen

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.