This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

CCS/TAS5754M: TAS5754 soft issue

Expert 1640 points

Replies: 3

Views: 206

Part Number: TAS5754M

Tool/software: Code Composer Studio

Hi Sir

could you help check above questions,tks!

Now there is no demo board. I use the following PurePath Studio (Home Audio) MiniDSP GDE software to edit the parameters offline, and generate the parameter cfg file such as attachment through Build-Generate Code. How is this file integrated into our software? could you help provide the way how to export register without connect  demo board

  7633.base_main_Rate48.cfgThe main question is how to write a piece of the following screenshot (no corresponding address?)?

  • Hi Darren,
    If you are using TAS5754M, why don't use PPC2 GUI for it? Are you doing this on the TAS5754M EVM please?
    Best regards.
    Shawn Zheng
  • In reply to Shawn Zheng:

    Hi Shawn
    because we do not have TAS5754M EVM in hand, so we use PurePath Studio GUI to generate the parameter cfg, wihch can finish it without EVM, However, the PPC2 can be generated cfg only in the condition of conncet with TAS5754M EVM , so we need you help provide the way how to export register without connect demo board by use PurePath Studio GUI,tks!
  • In reply to Darren Yang:

    Hi Darren,

    What's your major purpose?
    There is no way to finish audio tuning without a physical TAS5754MDACEVM connected.
    In addition, PPS (PurePath Studio) is not the recommended tool. PPC2 is!

    Andy

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.