This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

recommend DCDC design

Expert 1460 points

Replies: 4

Views: 147

Hi sir

our customer want to design above project about power, could you recommend suit for this Application IC and reference design,tks!

1: The input is 36~75VDC, the output power is 400W, 600W, 800W.
2: The input is 18~75VDC ultra-wide voltage input, and the power is 400W, 600W, 800W, which circuit topology is better.

  • Hi Darren,

    Could you please provide the output voltage for better to answer your question.

    Regards,
    Teng
  • In reply to Teng Feng:

    Hi Teng Feng

    output:12V-48VDC,however,maybe has 5V output  application,tks!

  • In reply to Darren Yang:

    Hi Darren,

    I want to see that the output voltage "12V-48VDC" you request is wide range output or a constant voltage value between 12V and 48V.

    Regards,
    Teng
  • In reply to Teng Feng:

    Hi Darren,

    I have answered your question in your another post.

    Best Regards
    Frank 

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.