This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TLV320AIC3104: TLV320AIC3104EVM : can't get analog input bypass to work

Intellectual 750 points

Replies: 11

Views: 545

Part Number: TLV320AIC3104

Hi,

I have a Texas TLV320AIC3104EVM board and am trying to connect the LINE2R input to RIGHT_LOP using the analog input bypass pathway as per section 10.4 of the datasheet.

So in the 'Bypass Paths' tab I select 'LINE2R - Bypass' which generates a message in the 'Command Buffer' tab :

            w 30 6C 80

As I understand the data sheet correctly, this should result in the signal I put into MIC2R/LINE2R coming out at RIGHT_LOP.

But I get nothing out which I don't know why.

The other issue is the command sent down the I2C, hex 80 is sent to register 108 but the data sheet, page 74, says bit 7 is reserved and bit 6 should be set to enable LINE2R bypass.

Is the data sheet in error?

Any help would be appreciated.

Regards,

  • In reply to Steve-Wilson:

    Steve,

    The answer did come as a bit of a surprise as the evm gui supported the bypass choice but at least we now know. We have rerouted our input to the LINE1L/R inputs.

    Thanks for your work on this.

    Regards,

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.