This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TAS5825MEVM: Cannot connect to TAS5825MEVM through PurePath console

Intellectual 495 points

Replies: 13

Views: 428

Part Number: TAS5825MEVM

HI,

I have just started work with the TAS5825MEVM and PurePath console motherboard.

I can connect (says 'connected' and green dot next to TAS5825M at the bottom left of the window), but when I try to run the hardware checks it fails. 

See screenshot below.

How do I get this to work?

  • In reply to Andy Liu SH:

    HI Andy,

    Does the TAS5756 not work with PPC3?

    Do I need a TAS5756 App for PPC2 (in the same way I needed the TAS5825 app for PPC3)?

    Can I have both PPC2 and PPC3 running / installed on the same PC?

    Regards,

    Ian Harvey

  • In reply to IanBristol:

    Hi Ian,

    See my comments below.
    Does the TAS5756 not work with PPC3?
    [Andy]: No, TAS5756MDCAEVM cannot work with PPC3. The only official GUI is PPC2.

    Do I need a TAS5756 App for PPC2 (in the same way I needed the TAS5825 app for PPC3)?
    [Andy] No. A few apps will be installed when the PPC2 is installed.

    Can I have both PPC2 and PPC3 running/installed on the same PC?
    [Andy] I have both installed on my 64-bit Win7 laptop, but they cannot run at the same time.

    Andy

  • In reply to Andy Liu SH:

    Thanks Andy,

    I will load up PPC2 and give this a try.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.