• TI Thinks Resolved

TPA2080D1: TPA2080D amplifier problems are as follows:1, when the volume is up to the maximum, the distortion is relatively large2. When the volume is up to the maximum, the IC works very hot3. When the volume is up to the maximum, the output of the amplif

Expert 1280 points

Replies: 6

Views: 143

Part Number: TPA2080D1

SCH-WSS_BM20L-V02.pdfTPA2080D amplifier problems are as follows:
1, when the volume is up to the maximum, the distortion is relatively large
2. When the volume is up to the maximum, the IC works very hot
3. When the volume is up to the maximum, the output of the amplifier is unstable

  • Hi Clark,

    I would like to ask a couple questions that might be related to the behavior you're seeing:
    - What is the speaker impedance you want to drive?
    - Did you followed the recommendations about boost inductor selection from data sheet page 16:www.ti.com/.../tpa2080d1.pdf

    If the rated current of the inductor is not high enough, the boost can turn unstable, mostly at high output levels.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators
  • In reply to Ivan Salazar:

    At present, we have changed inductances with larger currents of 1.5uH, 2.2uH, 3.3uH and 4.7uH, including inductance test of 6A current, without any improvement of distortion.

    The following inductance test instructions for 2.2uH

    1. The output frequency response and distortion curve of Bluetooth module are normal.

    2. Verify the output frequency response and distortion curve of the amplifier as follows:

    1. Speakers: 4R

    2. The tested supply voltage VBAT:4V

    3. The power supply VCC (VBAT) of the test power amplifier is 4V, and the PVDD is 5.4V.

    4. The oscilloscope is used to verify that the voltage is stable and there is no clutter. It is powered by a regulated power supply.

    5. AP-10dB input, power amplifier 2W output, no problem with frequency response curve

    6. Under the normal condition of voltage supply, the distortion curve should be greater than 1%, and the maximum is more than 5%.

    7. Not consistent with SPEC (VCC 3.6V, output distortion less than 1%) of TPA2080D1.

    8. Base noise is too high. Please help to list the optimization suggestions.

  • In reply to Ivan Salazar:

    I would like to ask a couple questions that might be related to the behavior you're seeing:
    - What is the speaker impedance you want to drive?----4Ω
    - Did you followed the recommendations about boost inductor selection from data sheet page 16:www.ti.com/.../tpa2080d1.pdf
    ---yes,At present, we have changed inductances with larger currents of 1.5uH, 2.2uH, 3.3uH and 4.7uH, including inductance test of 6A current, without any improvement of distortion.
  • In reply to Ivan Salazar:

    Can TPA2080D1 achieve 2.2W output power?

    At present, when the output power of our products reaches 2W, the temperature of IC is very high (abnormal), about 70 degrees.

  • In reply to Clark Li27:

    Hi Clark,

    The device is able to output 2.2W, this can be verified using an EVM. I tried this on my side and I get 2.2W into 4ohm at around THD+N = 1.1% with no excessive heating.
    Have you tried different speakers and also by removing the output filter? If something like this prevents the device heating then it would be related to the output loading.
    In addition, have you tried to use the same capacitor values as the EVM (1nF)?

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators
  • In reply to Ivan Salazar:

    Clark,

    Do you have further comments about my suggestions from previous post?

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators