This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] TLV320AIC CODECs and ADCs: What I2C speeds/frequencies are supported by the TLV320AICxxxx devices?

Mastermind 39175 points

Replies: 1

Views: 477

Hello,

Many of the TLV320AICxxxx and TLV320ADCxxxx datasheets refer to "standard" and "fast" I2C modes.  Can you confirm which speeds these correspond to?

Regards,
Collin Wells
Precision ADC Applications

  • These devices support standard (100kHz) and fast (400kHz) I2C speeds.

    Regards,
    Collin Wells
    Precision ADC Applications

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.