• TI Thinks Resolved

TAS5634

Prodigy 50 points

Replies: 1

Views: 45

Dear TI

       Can I use the TAS5634 for BTL output mode, the power is 2*100W, can the load be two 4 ohm speakers? Because I see the specification BTL mode is only 8 ohms and 6 ohms.

  • Hi user5875715,

    TI doesn't support using the device in 4ohms in BTL. There is a thermal constraint to running the device in BTL with 4ohms. 

    Now that said at low power levels the device can theoretically run the 4ohm load. But we can't guarantee the performance of the device in this configuration. 

    Best Regards,

    Robert Clifton