Hello,
Can anybody help me?
I have a problem with TAS5630; with /SD,/RESET and /OTW tied together. When I connect the load ( pure resistor 8 ohm) at a level of sinus of 27V rms TAS is going in SD state
I tried to reset it ,I stopped the power supply but no effect ( the /SD is in 0 state, READY is in 0 state,C_STARTUP is in 0 state
Power supply is at 43V - is a 60V/10Amps with current at maximum
I am using an extruded heatsink with brass spacers
First question - It is possible to test TAS without heatsink ? (no load). It is protected at over temperature ?
Second question - what are the possible reasons of destroying TAS? ( I tried to make the PCB like those recommended from TI ) The components are like in the demoboard ( are not 0605 dimension; are 0805 dimension) I am utilising for filtering 15uH ( ferrite core tested at 500 khz) working at max 5A with 0.68uF
Before the amplifier go down I have seen on my scope noise on the sinus ( at maximum and minimum of amplitude)
I thanks in advance for any help
Cornelx