This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] PGA4311: EVM GUI Problem

Mastermind 26420 points

Replies: 1

Views: 739

Part Number: PGA4311

PGA4311 EVM GUI Problem

Hi, I have a customer who is trying to get the PGA4311 EVM to work and keeps getting an error message. 

When I try to set up this EVM on a Win XP system (using sboc277a), i get the following errors too. 

And when I click on "Click Here", I see the following. 

Can anyone advise what I am missing here? 


Verified Answer: 

Hello,

I was able to reproduce the issue.  It appears that after installing the software, the user is required to manually replace the 'inpout.dll' from 12/04/1996 with the updated file 'inpout.dll' from 7/22/2003.  After installing the software, find in the sboc277a folder the Windows XP dll update 'inpout32.dll' file dated 7/22/2003 that needs to be manually saved in the folder:  */ProgramFiles/PGA2311EVM/ 

Attached are the instructions; and the sbocc227a with updated dll file.  Please let me know if this workaround does not solve the issue.  Please find the instructions below

sboc227a:

1307.sboc227a.zip

Installation Instructions:

2063.Installation Instructions-Important.txt

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.