Hi,
Need your good advice on PCM9211 registers setting on port group MPIO_C.
When MPIO_C is used as functions such as AUXIN1 or ADC or others other than DIR flags output or GPIO (register 6Fh), how should the register 71h be set?
It wasn't stated in the datasheet when this register is effective.
Whereas for registers 76h, 77h and 7Ah, it is mentioned that it is effective only when MPIO_C is assigned as DIR flags output or GPIO.
Thanks.