Hi Team,
I am working the above device, finding the SNR and THD values with Sine wave input (984.375Hz) input signal generating through AWG with 448KHz Sampling frequency.
In the Test Input signal pass through the Input Buffer, Mixer, PGA and then Map to Low power output pins through register setting.
We could read SNR values around 72dB and noise floor at -80dB.
Hardware detail: We have on board filter at Low power output pins with 10K resistor connected. with this resistor value we getting SNR 72dB, for experiment purpose change to 5K instead of 10K then we got 89dB SNR and noise floor at -110dB . please find the attached PPT for reference and let us know whether placing 5K resistor is allowed.
Thanks & Regards,
Sunil BK