This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA2013D1: Occasional circuit protection for large signal output

Part Number: TPA2013D1

Hello expert,

I am in charge of investigating the causes of trouble with TPA2013.
We use TPA2013(RGP) as an audio PA in our wireless radio product. The trouble is beep (key touch tone) at ful volume  could result in breakdown (functional suspension) of TPA2013 due to circuit protection, which recovers after reboot. It does never happen at lower volume. It does not occur in all the products and not always occur. But once the trouble occurs, the product seemingly become so fragile as to frequently cause the trouble, and finally TPA2013 is fatally damaged and broken.
Please have a look at the scheme. R6 in the scheme is the variable register. We do not use the boost converter part of TPA2013. I suspect VccFB pin (#2) can be left open even if the boost converter is disabled. Could you help me to find any other problems with our scheme?
Thank you for your cooperation in advance.

Ryoji

  • Hi Ryoji,

    Welcome to E2E, thanks for your interest in our devices.
    It seems that you are using Bypassing the Boost Converter configuration if so, You need to add R1 and R2 even if you are not using the Boost converter. I also recommend you to add decoupling capacitors at Vdd pin and they should be placed as close as possible to the device.
    Could you provide me more details when the problem happens? and Could you provide me measurements of the device when you can replicate this condition?

    Best Regards
    José Luis Figueroa
    Audio Applications Engineer
  • Hello Jose,

    Thank you for your quick reply.
    According to your advice, I additionally assembled 47kOhm and 470kOhm as R13 and R14 respectively, but unfortunately it had no effect on the trouble.
    As I wrote in the previous post, circuit protection or breakdown was caused by beep (1kHz or 400Hz) at full or near-full volume. The output pin (VO+ or VO-) of fatally broken TPA2013 turned out to be short-circuited to PGND.
    Here are measurements.
    Figure 1 shows signals at the inputs of TPA2013, pin #7 and pin #8 at full volume. When beep sounds, the input swings 1.4Vpp, which obserbes absolute maximam ratings of TPA2013. Beep sounds for 200ms long.
    Figure 2 shows a normal signal at the output to the transformer (at C13) at full volume . The peak-to-peak is about 4.5Vpp because R6 is changed to 4.7kOhm to avoid circuit protection.
    Figure 3 shows a signal at C13 when circuits protection occurs at full volume. The peak-to-peak is 7.5Vpp with R6 of 1kOhm (original value).

    If you need other measurements, do not hesitate to provide direction.

    Ryoji


    If you need other measurements, do not hesitate to provide direction.

    Ryoji

  • Hi Ryoji,

    I have additional questions. Have you added the decoupling caps at Vdd pin? and Do you know the power dissipation when the problem happens?

    Best Regards
    José Luis Figueroa
    Audio Applications Engineer
  • Hi Ryoji,

    I haven't heard back from you. I am assuming that you were able to solve your problem. If not, just answer my questions or create a new post if this was locked due to time-out.

    Best Regards
    José Luis Figueroa
    Audio Applications Engineer
  • Dear Jose,

    Sorry for my long blank. Unfortunately the breakdown problem of TPA2013 has not been basically solved yet.
    I tentateively changed R6 from 1k Ohm to 10k Ohm to increase loss of the beep. The countermeasure seems successful to prevent beakdown so far, but the root cause of the breakdown remains unclear.

    I marshaled the measurement results as follows.
    Figure 1 to 3 show input and output signal of TPA2013 using R6 of 10k Ohm, while Figure 4 and 5 show input and output signal of TPA2013 using R6 of 1k Ohm.
    All measurements are done with the volume maximum, but tempolary or parmanent breakdown did not occur during the measurements.
    Figure 1 and 2 both show beep at in+ and in- of TPA2013, with R6 of 10k Ohm. In Figure 1 the signals are DC coupled, while in Figure 2 AC coupled.
    Figure 4 shows beep at in+ and in- of TPA2013 in AC coupling with R6 of 1k Ohm. These figure shows signals do not exeed absolute maximum ratings of TPA2013.
    Figure 3 and 5 show beep at out+ and out- of TPA2013, measured at the terminals of T1. My concern is that amplitude of out+ and out- are not equal and balanced in both figures.

    We measured V-I characteristics of the broken chip. It proved that shortcircuit occured between PGND (9,10pin) and VOUT- (11,12pin). But we could not find any visible evidence of the shortcircuit in the micrographs of the chip of which plastic mold was removed.

    About your last questions, I have not add decoupling caps at Vdd pin yet. The only decoupling cap of 10 uF is placed at the 5.3V input of the PCB, 10 cm away from TPA5013. I will add some caps near TPA5013 and report the results. About the power dissipation, I never measured it but the output audio power of TPA5013 is about 1.5W.

    It would be very helpful if you provide me possible couse of the breakdown.

    Thank you for your help.

    Ryoji

  • Hi Ryoji,

    You must add the decoupling capacitors as close as possible to the Vdd pin in order to ensure a high-efficiency operation with low total harmonic distortion (THD). Besides, these capacitors avoid to get a high ripple on the power supply, and therefore, this also avoids high peaks on the PWM signal of the device's output.
    You could disconnect the transformer and output filter in order to review if the problem is produced for one of these components as you mentioned me that the device's outputs are damaged. You could perform the tests without these components to discard a problem with them.

    Best Regards
    José Luis Figueroa
    Audio Applications Engineer