Hi!
I'm working on a project where I need to convert an analog audio signal to SPDIF. I purchased the PCM9211 EVM evaluation board to explore this IC and try to make it do what I want. It turns out, I can't!
I've been searching all way, but I still haven't found out how to make this work.
My goal is to use the PCM9211 to convert analog audio to SPDIF without having to rely on other ICs such as the TAS1020.
I read somewhere on this forum that I had to connect the input and output i2s lines on the chip in order to "route" the digital audio back into the chip. I therefore connected pin 7 to 20, 19 to 8, 18 to 9 and 17 to 10, but I still haven't been able to make it work by using the CodecControl software.
Can someone help me with this by either helping me with a script or a screenshot along with a physical connection setup?
Thanks!