Hi Expert,
I used the below PFW to run AIC3262, but I can't hear I2S2. Should I add other command for it? Thanks!
PS. IN2L/R and I2S1 are OK!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Expert,
I used the below PFW to run AIC3262, but I can't hear I2S2. Should I add other command for it? Thanks!
PS. IN2L/R and I2S1 are OK!
Hi, Jerry,
It seems you are using I2S3 as the digital output interface (I2S_Out3), not I2S2. In general when either I2S2 or I2S3 are used in a process flow, the system settings code is updated to enable the corresponding interface.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer
Hi, Jerry,
Thanks for the feedback. The interfaces should be programmed automatically, but just to make sure, can you please send me the .cfg file generated in your application for review?. Can you please also confirm if I2S3 is working well?. I assume you are using an EVM, if so, can you please share the connections you are doing to the interface I2S2?.
Best Regards,
-Diego Meléndez López
Audio Applications Engineer