This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320AIC1106: TLV320AIC1106 select LINSEL Pull high, no sound issue

Part Number: TLV320AIC1106
Other Parts Discussed in Thread: TLV320AIC3101

Dear,


our client design TLV320AIC1106 with MC8090( 3G Modle) was can work and sound  was normal , but MC8090 was EOL.


so We change Air prime  WP8548( 3G Modle) linear mode  Audio sound was no clearn have backgounf noise, select 8 bit u-law mode was no sound.

have any suggestion other Audio code with  the same TLV320AIC1106 spec, but can support 16 bit linear.

schematic:

3G Audio PCM SCHEMATIC.pdf

If any, Please advise me.


Thanks,


Best regards,


Lawrence.

  • Lawrence,

    There are a number of codecs that have similar spec, but not exact, and the pinout will be different.

    1. TLV320AIC23B - This is another simple codec, but it is not hardware controlled, I2C is required to program it. headphone out supports 32ohm minimum
    2. TLV320AIC3101 - This device is much more flexible. and has more inputs/outputs.

    Best regards,
    -Steve Wilson
  • Hi, Steve

    TLV320AIC1106 we saw can support 13L and 8u law mode , our client use PCM interface as below spec, it could be workable?

    if any suggestion, Please advise me.

    Thanks,

    Best regards,

    Lawrence.

  • lawrence,

    Can you explain the volume padding bits?
    all of TI's more recent (2003-present) audio codecs will used 2's complement data. to be clear, this is all PCM data, and not PDM.

    best regards,
    -Steve wilson