Dear Specialists,
My customer is considering TPA3220 and has questions.
I would be grateful if you could advise.
---
In the data sheet p24 Figure 44., In the configuration of Mono BTL, we designed a circuit with monaural 4 Ω and instantaneous maximum 10 W rated 5 W.
According to p16 9.2 Functional Block Diagrams,the H bridge power supply of each channel is independent,
(1) Is it necessary to connect only the PVDD terminal (pin 37, 38, 39) of the OUT1 channel to the electrolytic capacitor and the ceramics?
Is it unnecessary to connect a capacitor to the OUT2 channel when is not used?
Are these correct?
(2) Is it necessary to supply to PVDD (pin 30, 31, 32) of the OUT 2 channel when is not used?
---
I appreciate your great help in advance.
Best regards,
Shinichi