This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

PCM2903C: AND gate in PCM 2903C

Intellectual 650 points

Replies: 1

Views: 90

Part Number: PCM2903C

Hello Sir

I'm using PCM2903C in my project. The typical application circuit mentioned in datasheet contains an AND gate. Why that AND gate is used?

Please help me out in this concern.

Regards

Nidhi P Shetty

  • Hi, Nidhi,

    The AND is used to pull-up D+ signal only when both Vbus and VDD are provided to the device.  As this part is not USB-powered, this method is used to make sure the part is not active until the relevant supplies are stable.

    Best Regards,

      -Diego Meléndez López
       Audio Applications Engineer

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.