This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

TPA3244: Unused channels

Expert 6675 points

Replies: 1

Views: 91

Part Number: TPA3244

Hi Team,

If I am configuring the TPA3244, what should i do with inputs and output that are not used? If I am driving one speaker or transducer with a single-ended output, should I ground the unused inputs and outputs, or leave them floating?

Any guidance you can provide would be greatly appreciated.

Thank you!

Jared

  • Hi Jared,
    If only one channel is used, you could set the amp in PBTL mode - Figure 25 and Figure 26 in the datasheet show this kind of application. If you still want to use the device in BTL mode(Figure 23), you could remove the output circuit on the unused channel but keep the bootstrap caps.
    Best regards,
    Shawn Zheng

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.