Dear all
The Slau232.pdf said: "The default configuration will provide power, control signals, and streaming audio via the USB interface from the PC."
I want to know how to set the streaming audio via the USB interface from the PC ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear all
The Slau232.pdf said: "The default configuration will provide power, control signals, and streaming audio via the USB interface from the PC."
I want to know how to set the streaming audio via the USB interface from the PC ?
Went,
SLAU232 is for the AIC34. The Correct users guide for the AIC3104 is here.
Table 1 in this user guide explains the positions of the switches on the USBMOD-EVM SW2.
For use with the TLV320AIC3104EVM, SW-2 positions 1 through 7 should be set to ON, while SW-2.8 should be set to OFF.
With these settings the USBMOD-EVM will show up as an Audio Device in windows, and you can choose it for playback or as an input for recording.
best regards,
-STeve Wilson