Dear all,
One of my AA is going to use the TAS5421-Q1 to drive 15W in 8 ohm load. The TAS5421-Q1 will be supplied with 18V.
From voltage output point of view it seems that the TAS5421-Q1 should have the headroom to drive the 8ohm @15W.
Which could be the expected THD+N ? The application require a THD+N less than 1%.
regards,
Domenico