Other Parts Discussed in Thread: OPA1612
I have a design that is currently being manufactured using two PCM1794A chips in monaural mode. The THD+N varies drastically between boards and even between left and right channels on the same board.
The datasheet lists a THD+N of -108dB as the nominal but there is no min or max listed.
My question is how much can it be different from chip to chip. I am seeing between -101 and -111dB between different chips, is this normal or is this some kind of weird manufacturing error that is going on?
Here is what the output circuit looks like, it uses 0.1% resistors and 1% COG capacitors.