Hello, i would like to know some tips to design properly some boards implementing tpa3255 and tpa3116 chips.
First, on the tpa3255 datasheet, for the stereo btl application, is the circuit operational? By operationnal, i mean, could a board exactly designed like the one shown can work, without the "fancy" or extra fonctionalities used (like those allowed with the pins: OSC_IOM, OSC_IOP, RESET, FAULT and CLIP OTW) i know that i can leave the osc pins unconnected, but for the reset, fault and clip otw pins, could i just ground them or leave them unconnected, if yes, which ones ?
For the tpa 3255, can i use a separated power supply for the 12v entry (dedicated to the low power circuitry) that is independant of the high voltage one, so that is not coming from the high power supply by being regulated but with a distinct transformer (can this transformer be unregulated, but just rectified with big reservoir capacitors to have the most linear voltage as possible)?
Also, is it possible to synchronize multiple tpa3255 board to each others? If yes, how far can this go?
For the tpa3116 boards, also can it is possible to combine more than 2 board all togethers, if yes how?
For the tpa3116 design one the datashep version, there is only one 100k resistor going from sdz and faultz pins to pvcc, while the modsel is going directly to ground, on the evaluation board there is a distinc 100k resistor for each of those pins, it's (i assume) for testing purposes, but did i have to apply the datasheet or evaluation configurations for best results?
For the tpa3116 design, if i use only one board and i don't want to connect it to another device, could i juste have to simply connect this pin to ground or make a rc filter (with a 4,7k resistor and a 47pf capacitor) on this pin, like it is done in the evaluation module ?
I really would like to know if the fact of using trough hole rather than smd components affect the sound quality of the system ? I know that trough hole metal film resistor generate less noise than smd resistor, but, for the capacitors used, i know that plastic film capacitors are usually better in all aspects of performance, with no taking care of the cost and the size, but, comparatively, they prone to pickup more rf noise than the smd ceramic capacitors (who are smaller). So what is the best, what is the advantage of those smd components over those old through hole components (other than cost and size)?
Finally, according to users who tried tpa3116 and 3255 board, all of them said that the tpa3255 chip is really better; despite the higher power output and the better snr ratio of the tpa3255 (that is a sound quality factor, among others), for low volume listening (using no more than 20w of power by example, so the tpa3116 does not generate audible distortion) is the tpa3255 really better?
Thanks for your futures reply to my (relatively) dumb questions, i tried my best to formulate them and i hope that you can respond to them!