Hello,
Would you please tell me how to disable the clock output from OSC_SYNC pin in master mode? It has output even when configuring 0x0A[6]=0 and 0x0B[7]=0, so it doesn't seem to work as shown in the datasheet.
Best Regards,
Kawasaki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Would you please tell me how to disable the clock output from OSC_SYNC pin in master mode? It has output even when configuring 0x0A[6]=0 and 0x0B[7]=0, so it doesn't seem to work as shown in the datasheet.
Best Regards,
Kawasaki
Kawasaki-san,
In Table 19, the default is that the clock is not present on the OSC_SYNC pin. It must be enabled by the software if you need a clock on this pin. You need to do nothing, if you do not need a clock.
Hello Gregg,
Thank you very much for your comments. Do you mean 0x0B[7]=1(default) is disabling the clock output(0x0B[7]=0 is enabling the clock output) even though the datasheet looks 0x0B[7]=1(default) is enabling the clock output? I'll ask my customer to confirm that.
Best Regards,
Kawasaki
Hello Gregg,
Thank you very much for your comments again. It seems the output from OSC_SYNC when 0x0A[6]=0x0B[7]=0 has around 40mVpp as shown below. Do you think it's normal by the register settings? My customer expected almost 0mVpp output. Note that their system configures Fs=417kHz.
Kawasaki
Kawasaki,
The normal output signal when turned on is 3.3Vpp. If you are seeing this small voltage, it is probably leaking through and you are measuring it. It will not be an issue.
Hello,Gregg.
I ask you a question by addition for a question of Kawasaki.
A leak of the Clock waveform was observed by OSC_SYNC terminal.
It is the waveform of the internal clock which the waveform which Kawasaki attached leaks out to.
As for the frequency, 3.33MHz, voltage are 58mVpp.
fS sets it to 417kHz.
The Clock output becomes the halt setting.
Please tell me the manner to evade it because I influence EMI performance.
Best regards,
Murakami
Hello Gregg,
It seems my customer has EMI issue which would be caused by that. I'll ask you by email because you may need NDA information to fix this.
Best Regards,
Kawasaki