Hi,
Would you please help on shematic review? Also I want to confirm following things:
1. Configuration of automatic fault shutdown and Mute controls are correct?
2. Is FaultZ open drain output?
3. In figure2, what is the meaning of 1.4 second? Does it mean when device detect short current and and SDZ is directly connected with FaultZ, then faultZ outputs low signal . The device need more than 1.4 second to shutdown?
4. If there is a special design to suppress pop sound?
Thanks!
Figure 1
Figure 2