This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV320DAC3120: What is the input resistance of AN1 and AN2?

Part Number: TLV320DAC3120

What is the input resistance of AN1 and AN2 in TLV320DAC3120?  If not resistive, please provide detail on input impedance vs. frequency.  Thx.

  • Hello!

    The input resistance of AIN1 and AIN2 depends if only one or both AINx inputs are routed to the output mixer.

    Typically, if only one AINx input is routed, the impedance will be around 11.2KOhms. However, if both inputs are routed, the effective impedance will down to 5.6KOhms.

    Best regards,
    Luis Fernando Rodríguez S.