This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

LM48511: LM48511 Can drive 8Ω 1.5W Speaker?

Intellectual 430 points

Replies: 1

Views: 64

Part Number: LM48511

hi TIer,

    Could you please help to check if LM48511 can drive 8Ω 1.5W speaker and how to set the parameter of LM48511,TKS.

  • Hi Jerry,

    Data sheet specifies that LM48511 is able to output 3W into 8ohm load at 1% THD+N when powered by 5V.
    LM48511 is an analog input amplifier and hardware controlled; what parameters are you asking for? You can use the recommended component values from typical application circuit, and also check section 8.2.2 if you want to select different component values.

    Best regards,
    -Ivan Salazar
    Applications Engineer - Low Power Audio & Actuators

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.