This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] TLV320AIC CODECs: What is the maximum output load capacitance on the headphone amplifier outputs?

Mastermind 41955 points

Replies: 1

Views: 438

What is the maximum output load capacitance on the headphone amplifier outputs?

Regards,
Collin Wells
Precision ADC Applications

  • It is not recommended to place any loads with a capacitance higher than 200pF directly on the headphone outputs. Higher output capacitances can be tolerated by placing a series resistor between the output and the capacitive load.

    Regards,
    Collin Wells
    Precision ADC Applications

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.