This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[FAQ] TLV320AIC3104: Line Out - Output Impedance

Part Number: TLV320AIC3104

What is the output impedance of the line outputs in the TLV320AIC3104 device?

  • We don’t specify or production measure the output impedance of the line outputs but when powered up the line outputs should be on the order of 100 Ohms and the high power outputs should be less than 1 Ohm. When these outputs are in High-Z, they should be greater that 50 k Ohms. This would be over the full audio band.