This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] TLV320AIC23: Pinout of the TLV320AIC23

Mastermind 40900 points

Replies: 1

Views: 404

Part Number: TLV320AIC23

The BGA pinout of from page 1-4 seems to contradict the package drawing on page A-1.  Can you help clarify the pinout?

Regards,
Collin Wells
Precision ADC Applications

  • Both diagrams are correct. Unfortunately, they use a different numbering convention. The drawing in Appendix A is using rows (alpha) and columns (numeric) whereas Page 1-4 simply numbers around the edges.
    Page 1-4 is a top down view and has the correct pin numbering. Appendix A is a generic BGA using a different numbering system. So, pin 2A from appendix A would correspond to pin 32 on Page 1-4.

    Regards,
    Collin Wells
    Precision ADC Applications

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.