This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] PCM2912A: Driver requirement for using device on OS

Expert 5655 points

Replies: 1

Views: 554

Part Number: PCM2912A

Do we need any special drivers to use PCM2912 device on OS?

 

Best regards,
Ravi

  • NO.
    PCM2912A is a USB-audio codec which uses the native USB Audio Class driver from the host Operating System. There is no need for an extra driver to operate with Linux or other OS as the UAC driver should be part of the OS.


    Best regards,
    Ravi

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.