This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

[FAQ] PCM9211: Using device with no XTAL

Expert 5655 points

Replies: 1

Views: 724

Part Number: PCM9211

Can the PCM9211 be used without the 24.576 input clock? 

 

Best regards,
Ravi

  • YES. PCM9211 can be used without external crystal. DIR/DIT & ADC can operate without XTI clocking. However, running without the XTAL has limitations including

    • No fs estimation

    • fs range is 28K-108KHz only, no support 192KHz.

    Best regards,

    Ravi

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.