This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TAS5634

Other Parts Discussed in Thread: TAS5634

Dear TI

       Can I use the TAS5634 for BTL output mode, the power is 2*100W, can the load be two 4 ohm speakers? Because I see the specification BTL mode is only 8 ohms and 6 ohms.

  • Hi user5875715,

    TI doesn't support using the device in 4ohms in BTL. There is a thermal constraint to running the device in BTL with 4ohms. 

    Now that said at low power levels the device can theoretically run the 4ohm load. But we can't guarantee the performance of the device in this configuration. 

    Best Regards,

    Robert Clifton