This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DIX4192-Q1: What's the difference between DIX4192-Q1 and DIR9001-Q1 regarding the receiving function?

Part Number: DIX4192-Q1
Other Parts Discussed in Thread: DIR9001-Q1, , DIR9001, DIX4192

What's the difference between DIX4192-Q1 and DIR9001-Q1?

we a little bit confused because the datasheet format is different.

I need to know like what DIX4192-Q1 can do and what DIR9001-Q1 can't do.

Can you provide the comparison table between these two device regarding the receiving function(DIR)?

  • Hello Uozu-san,

    We will get back with you on this soon.

  • Uozu-san,

    Actually this will take a deeper investigation.  Please give us up to one week.

  • Hello Uozu-san,

    The DIX419x devices were actually released about 8 months before the DIR9001 and they do not share the same receiver interface for the S/PDIF signal inputs.  The DIX4192 utilizes a differential input receiver while the DIR9001 implements a single-ended receiver.  The DIR9001 therefore would require some additional circuitry if it’s meant to receive a small-signal differential signal like the DIX4192 can accept.  A similar circuit can be seen in Figure 14 of the DIX4192 datasheet.

     The DIR9001 is compliant to the jitter and other IEC specifications, but does not implement a differential RX signal path like the DIX4192 which looks to be more fully compliant with differential input level IEC specifications as well.