Hello!
I am using TAS2557 working as a master on I2S (WCLK 44.1kHz, BCLK 1.4MHz ,16bit) in ROM Mode 1.
My TAS2557 is a part of an embedded system running on a 1.5V battery, so naturally i want the TAS2557 to consume as little power as possible while not playing audio. So, when there is no audio to be played (i know this in my program) i want to put the TAS2557 in "Low power sleep mode" or use a "power down and mute" sequence. And when there is audio to play, i want to wake up the device again.
Whenever i try to write the example presented in the datasheet, the clocks generated by TAS2557 (WCLK and BCLK) shuts down and the power consumption is significally lowered. But whenever I try to power up the device again, nothing is happening.
So my question is: What sequence of commands do i need to send in order to get the device to power down and power up somewhat quick? I dont want to re-initialize the device all over again.
I don't necessarily need the absolute lowest power consumption possible. The time it takes to power down/power up is more important.
Thank you in advance,
/Viktor