1. Project Background:TLV320DAC3101IRHBR is used for the project of DOCKING connectd to mobile phone by TYPEC3.1 cable. I2S audio of TLV320DAC3101IRHBR is separated from DISPLAY singal. Speaker is 2-W, 4-Ω speaker. Register parameter is writed in chip by I2C of other chip for no driver.
2. Issue A:When I Adjust the volune from 100% to 0, the horn sound become very small about 50%. Result of a measurement sperker is as follow, when phone play 1Khz voice.
100% : peak-to-peak value of speaker is 6.2V. 50% : peak-to-peak value of speaker is 1V