Hi
We are doing 192KHz sampling rate audio and need 20 ~ 96KHz flat frequency response.
Can you help for the output filter circuit ? thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
You may try with 3.3uH inductor+0.47uF cap.
BTW, slaa701A is a good reference for LC design.
http://www.ti.com/lit/an/slaa701a/slaa701a.pdf?keyMatch=SLAA701A&tisearch=Search-EN-everything
Regards,
Hao
Hi PYTsai,
We forgot to mention that another thing that's important to take into consideration with the TPA3255 is the minimum inductance for the LC filter inductor is 5uH!
I would still recommend reading into the LC design that Hao recommended as things like the load's resistance will also be a factor in the frequency response curve.
Best Regards,
Robert Clifton
Hi Robert,
thanks for your remind and suggest.
customer tried 5.1uH+0.47uF, the red light of the EVM board was directly lit, and it could not operate normally.
We also tried 7.1uF+0.47uF. When the input power is small, the output characteristics are not normal, the frequency response is not consistent with the calculator,and there is attenuation at 20KHz.
In addition,test of 7.1uF 1uF the output stable,the frequency response is the same as the calculator but However, there is still attenuation at 20 kHz.
The above tests are all directly using APx525, without passing through the AUX-0025 filter.
have any idea or suggestions?
Hi Tommy,
Though a 5.1uH inductor is above the minimum, inductors always have tolerances and those particular ones likely were less than 5.1uH thus causing the immediate fault light going off.
Can you send me pictures of the output waveform so I can see what you mean by the strange output characteristics? Also what frequency was the input signal when you saw this? What was the Vrms of the input signal? Are you using any of the AP filters?
More information on your setup will help me better debug this.
Thanks,
Robert Clifton
Hi Robert,
I'm Elytone electric engineer, Eric.
Actually, we have measured the inductance value by RLC meter, the inductor is 5.2uH.
We also tried 7.1uH+0.47uF and 7.1uH+1uF, we couldn't get the same frequency response curve with LC filter designer.
Below is our detail setting for EVM and AP.
EVM Setting:
Single end input
2xBTL output
4ohm load
AP Setting:
No filter, Bandwidth=90KHz(192KHz SR)
At this case, the frequency response is attenuated at 20 kHz.
2. Our test result is different with the LC filter designer(30KHz no decay by calculator).
Anyway, the main problem is that we couldn’t find a set of value for LC filter to make a flat frequency response from 20Hz to 100KHz.
Thanks.
BR,
Eric
Hi Eric,
Looks like we have multiple things going on here.
Did you test the output's THD+N with the default inductors attached? If the THD+N looks better with those inductors that would indicate that the inductors that you've chosen are adding noise. Could you provide a THD+N vs Power graph? That would help me get a better idea of the curve.
It would be difficult to get a completely flat frequency response but it would be possible to get it to where it will drop less than -1 dB of gain at 100kHz. Does the system have to be completely flat or is there a certain amount of loss allowed?
Regards,
Robert Clifton
Hi Robert,
Yes, we can get the test result which similar with the datasheet after we changed to default LC.(10uH+1uF).
I have attached THD+N VS Power graph for 7.1uH+0.47uF and 7.1uH+1uF. The poor THD+N only exists on 7.1uH+0.47uF, and we tried different bandwidth AP setting, the problem only exists on the 192K bandwidth setting. I think that should not the inductor's problem. It looks like other limited factor of the LC combination when system on 192KHz bandwidth.
7.1uH+0.47uF
7.1uH+1uF
About the frequency response, we know that is difficult to achieve flat curve to 100KHz.
Our requirement is +0/-3dB at 20~100KHz, just like the below calculator picture. But now we couldn't get the same curve when we applied the same LC values on EVM.
Hi Eric,
I was a little confused on what the issue was! This is very strange indeed. It's almost as if the signal is getting buried by noise but then abruptly returns to what we would expect to see. I would start by double checking the signal chain to make sure that everything is clean. I noticed that the low frequencies had a rise in THD+N. Was this observed with the 7.1uH + 0.47uF filter?
Are you generating the input signal with the AP? If not what are you using? If you are using the AP to generate those signals would you be able to try testing the input by switching to a differential input signal to see if this removes what you are seeing when the signal is small?
Regards,
Robert Clifton
Hi Robert,
Yes, we used AP to generate the input signal, I will try the differential input then back to you.
There is another urgent question need to be check. Can we get a set of LC values to achieve 20~100KHz +0/-3dB frequency response?
Although we solved the THD+N issue for 7.1uH+0.47uF, it still couldn't meet our FR requirement.
If you have the TPA3255 EVM, could you please test and provide a set of LC values for 20~100KHz +0/-3dB frequency response first?
Thank you.
BR,
Eric
Hi Eric,
This is strange. I think we will need to do some testing on our side to determine the root cause. Can you tell me the EVM configuration? I want to know all of the jumper settings as well as the part numbers for the inductor you are using and the capacitors.
Thanks,
Robert Clifton
Hi Eric,
Can you also provide the LC part numbers you used?
Thanks,
Robert Clifton
Hi Robert,
Inductor: Coilcraft MA5172-AE 10uH (We reduced the wire round then measured the inductance through Chroma LCR meter for current testing.)
Capacitor: EPCOS B32652A3474K000(0.47uF) and Kemet PHE426HB7100JR06 (1uF)
We found the 4ohm dummy load which with around 18uH inductance, that is why we couldn't get the same curve with the LC calculator table.
We have changed another 4ohm dummy load(inductance =0.3uH) and re-test again, now we can get the correct curve. But the THD+N issue is still exist on 7.1uH+0.47uF.
We also tried to change back to 5uH+0.47uF. It can be powered on normally, but the fault LED always lighted when I did THDvsPower testing.
Hi Eric,
Well it looks like at the lower signal levels, the THD+N vs Power curve looks normal than jumping up high. This was all as a result of changing the load to be less inductive.
Are the frequency responses of both filter configurations within the range that you are wanting for your system?
Regards,
Robert Clifton
Hi Robert,
The frequency response of 7.1uH+1uF looks fine for us, and this setting without THD+N jump to high issue, thanks.
Now we have another problem, I couldn't reproduce the THD+N test result as datasheet even though we use the original filter(10uH+1uF).
Could you help to check anything we may missing? Our requirement is under 0.01% for 0~100W.
TPA3255 Datasheet Page 10
EVM ( BTL2.0, 36Vin, Differential input, L=10uH, C=1uF, AES17+AUX-0025)
Hi Eric,
THD+N is very dependent on the inductors. I've seen inductors that all have the same value but have wide variety of THD+N performance.
Regards,
Robert Clifton
Hi Eric,
Just noticed even on datasheet curve, THD+N could go above 0.01% at 25W and 75W. It may be very hard to achieve THD+N<0.01% in 0~100W...
Regards,
Hao
Hi Hao,
Got it, we will discuss with our customer for the THD+N specification base on what we can achieve now.
Thanks for your reply.
BR,
Eric