Other Parts Discussed in Thread: SRC4392
Dear engineer,
We decide to develop a HIFI DAC with PCM1794 but meet some theoretical problem.
It is easy to provide PCM1794 with an accurate SystemClock, frequency of which is more than100 times larger than clock of I2S.
But clock accuracy of I2S is unstable. e.x sometimes time length of high-voltage signal is shorter (maybe 1or2 clock cycle of SysClock). if I2S interface input a "1010"digital signal, but the length of both 1 are 127SysClock cycle while the length of both 0 are 129SysClock cycle, will PCM1794 correct the jitter to be ideal signal which are all 128SysClock cycle long?
If such Jitter of I2S signal cannot be corrected by PCM1794, is there any suggested method to Reorganise clock of I2S signal?
Thank you!