Hi, we met a problem that TLV320DAC3100 cannot drive a 8ohm speaker. SW investigation shows there is overcurrent event occurred. There are two 100nF capacitor pararlled on SPKOUT+ and SPKOUT-. This issue didn't show on our LP1 board, but it shows on recent LP2 board. The difference between the two boards are on LP2 the SPK+ SPK- trace is widen from 4mil to 15mil, and the filter capacitor keeps 100nF but package is changed from 0603 to 0402.
The voltage on SPK+ and SPK- output on LP1 is captured as this:
On LP2 board, the output waveform is as below, the SPK+ and SPK- keeps high for a long time(around 160us) then turns off, after that there is no more output:
Please advise what is the over current threshold of the driver, and what possible reason cause the issue?