Hi Team,
I'm wondering when I need to select low (100 mA) or high (500 mA) for the POWER pin. Is there a way to calculate total power consumption?
Thanks!
Roy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Roy,
This is largely going to depend on what your DAC output load is since that's where most of the current goes. The power consumption is specified for an RL = 32Ohms, but if for example you were driving a 16 Ohm load then you may want to operate in high power mode.
The Micbias and REC/PLAY LEDs may also contribute a bit, but the DAC output will still be the dominant factor.
Best,
Zak