Other Parts Discussed in Thread: TAS2505
Hi TI-team
I saw "TAS2505 Application Reference Guide".
There is a description of ”Reserved. Don't write any value other than Reset Value. ” on the ”Page 1 / Register 2: LDO Control Register - 0x01 / 0x0” on page 70.
However, in ”# LDO output programmed as 1.8V and Level shifters powered up. (P1, R2, D5-D4=00, D3=0)" of P.51, “W 30 02 0” is written to register.
Is there no problem ?
Best Regards,
Koji Hayashi